MQX 4.0.2 Telnet Server missing characters?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.0.2 Telnet Server missing characters?

2,039件の閲覧回数
wcampbell
Contributor I

I'm attempting to use the built-in MQX 4.0.2 (RTCS v3.08.00) telnet server on a V4 Coldfire 54415, but I'm running into a problem where it's losing data. I'm creating my task with TELNETSRV_init, and it is launching the task when I initiate a telnet connection to the device. In my task, I'm doing a loop that calls fgetc to grab each character, but only every other character is actually hitting my handler. The missed characters are being echoed back to my terminal program, but I can't find the source of the echo (I have echo turned off, and the characters that do hit my code are correctly not sending an echo). I don't even see the missing characters hitting the _io_telnet_read in telnetio.c. Has anyone else seen this behavior? Any suggestions on where I can look to see what's grabbing these extra bytes?

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,720件の閲覧回数
wcampbell
Contributor I

And (of course) minutes after posting this, it occured to me that an ECHOSRV is also being launched. It appears those two are fighting over data. I'm going to look into this more. This is very strange, since the echo server should be running on port 7. I'm going to have to dig into this more to see if I can find a reason for the two fighting over data.

0 件の賞賛
返信

1,720件の閲覧回数
Martin_
NXP Employee
NXP Employee

1) Change the echosrv application to use RTCS_selectset() instead of RTCS_selectall().

2) fix the RTCS_selectset() behavior per the instructions on the link below:

https://community.freescale.com/thread/321233