MQX 3.8.1 v1.1 installer - only change is in batch file?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 3.8.1 v1.1 installer - only change is in batch file?

跳至解决方案
846 次查看
dmarks_ls
Senior Contributor II

I noticed that the installer for MQX 3.8.1 was revved to v1.1 (20 Aug 2012), so I pulled it down, installed it, and compared it to a previous installation.  It appears that the only substantive difference between the two installs is that there is a "Workaround for morpho plug-in problem" in tools\codewarrior_extensions\CW MCU v10.2\install_cw10.2_plugin.bat.  (Well, that, and USB header files are now present in \lib for several different tower kits.)  Am I correct in that the batch file is the only change between v1.0 and v1.1 of the MQX v3.8.1 installer?

 

0 项奖励
回复
1 解答
696 次查看
DavidS
NXP Employee
NXP Employee

Yes, the only difference is the batch files.

The batches files are used to install CW 10.2 project wizard. The batches files will not work if the update 1.0 was applied to CW 10.2… We have to update the batch files to work around it.

There was a bug in the initial batch files, but only the CW 10.2 update revealed the bug. We raised the issue to CW team that CW can not break the existing releases out there… but sometimes it does happen…

在原帖中查看解决方案

0 项奖励
回复
1 回复
697 次查看
DavidS
NXP Employee
NXP Employee

Yes, the only difference is the batch files.

The batches files are used to install CW 10.2 project wizard. The batches files will not work if the update 1.0 was applied to CW 10.2… We have to update the batch files to work around it.

There was a bug in the initial batch files, but only the CW 10.2 update revealed the bug. We raised the issue to CW team that CW can not break the existing releases out there… but sometimes it does happen…

0 项奖励
回复