MQX 3.8(.1?) using with PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 3.8(.1?) using with PE

ソリューションへジャンプ
2,552件の閲覧回数
GerasinIvan
Contributor II

Hi all!

I have some problems with using MQX. To introducing into MQX, i used pe_demo. But after "build" i met an error:

#error Demo requires Processor Expert BSP code to be generated.

#error See "<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert" for details

in community i found

Re: Porting Kinetis BSP_pe from MQX 3.7 to MQX 3.8.1

But isn't really helps. So, i need step-by-step instructions to make and launch MQX on kintis. And how i can use PE in this project)

Thx for helping)

タグ(3)
0 件の賞賛
返信
1 解決策
2,373件の閲覧回数
Martin_
NXP Employee
NXP Employee

Hi Ivan,

"<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert"

on page 46 there is step 4 "Generate code"

First command PE to Generate code, then build.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,374件の閲覧回数
Martin_
NXP Employee
NXP Employee

Hi Ivan,

"<MQX_INSTALL_DIR>\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf" chapter "CW10.x, MQX and Processor Expert"

on page 46 there is step 4 "Generate code"

First command PE to Generate code, then build.

0 件の賞賛
返信
2,373件の閲覧回数
GerasinIvan
Contributor II

Thank you, Martin! It really helps. Now I can work with MQX, i hope) I will fully test it later, but i think it's all right. Thank you, again.

0 件の賞賛
返信