MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

ソリューションへジャンプ
3,291件の閲覧回数
juanee
Contributor III

Hello All,

 

I just installed Codewarrior 10, the special edition.  Is the TAD supported on this edition?

 

I searched the documentation for CW 10 and MQX 3.6.2 and I couldn’t find any information.

 

Thanks,

Juan

 

 ...

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

0 件の賞賛
返信
1 解決策
2,074件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,075件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

0 件の賞賛
返信
2,074件の閲覧回数
banjaxed
Contributor I

The whole area of CW and MQX is confusing enough without statements like this that are just downright WRONG.

 

Task-Aware Debugging is NOT available in the Standard Suite.

TAD is only available in the Professional Suite.

 

0 件の賞賛
返信
2,074件の閲覧回数
juanee
Contributor III

Thank you for your reply.

Juan

0 件の賞賛
返信