MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

Jump to solution
3,333 Views
juanee
Contributor III

Hello All,

 

I just installed Codewarrior 10, the special edition.  Is the TAD supported on this edition?

 

I searched the documentation for CW 10 and MQX 3.6.2 and I couldn’t find any information.

 

Thanks,

Juan

 

 ...

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

0 Kudos
Reply
1 Solution
2,116 Views
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

View solution in original post

0 Kudos
Reply
3 Replies
2,117 Views
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

0 Kudos
Reply
2,116 Views
banjaxed
Contributor I

The whole area of CW and MQX is confusing enough without statements like this that are just downright WRONG.

 

Task-Aware Debugging is NOT available in the Standard Suite.

TAD is only available in the Professional Suite.

 

0 Kudos
Reply
2,116 Views
juanee
Contributor III

Thank you for your reply.

Juan

0 Kudos
Reply