MQX 3.1.0 fails to compile with RTCS but without MFS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 3.1.0 fails to compile with RTCS but without MFS

Jump to solution
3,266 Views
gmabey
Contributor I

Hello,

 

I am compiling the BSP for M52259demo for the first time, and didn't make it very far.

 

After editing user_config.h and opening build_libs.mcp, I got this error:

 

 Error   : undefined identifier 'IO_IOCTL_CHECK_DIR_EXIST'

ftpd.c line 220               error = ioctl(session_ptr->CURRENT_FS, IO_IOCTL_CHECK_DIR_EXIST,(pointer)FTPd_rootdir );    

 

Error   : undefined identifier 'IO_IOCTL_CHECK_DIR_EXIST'

ftpd.c line 220               error = ioctl(session_ptr->CURRENT_FS, IO_IOCTL_CHECK_DIR_EXIST,(pointer)FTPd_rootdir );    

 

 

Upon examining the source code, it looks like the intent was to allow for compilation of RTCS without MQX, but I don't see evidence of support for RTCS without MFS.  

 

Is that a valid assumption?

 

Thanks,

Glen 

0 Kudos
Reply
1 Solution
1,988 Views
gmabey
Contributor I
Thank you, PetrL.  

View solution in original post

0 Kudos
Reply
2 Replies
1,988 Views
PetrL
NXP Employee
NXP Employee

Hi Glen,

 

it is bug in 3.1.0.

 

Description : In case FTPDCFG_USES_MFS is set to 0 in MQX user_config.h all references to MFS have to be leave out from compilation. Ftp server root directory is of such cases.

 

Problem will be fixed in 3.2.0 but in meantime you can fix it in if you use following version of ftpd_task function in ftpd.c file :

/*TASK*-----------------------------------------------------------------
*
* Function Name    : FTPd_task
* Returned Value   : none
* Comments  :  FTP server.
*
*END*-----------------------------------------------------------------*/

void FTPd_task
   (
      pointer  init_ptr,
      pointer creator
   )
{ /* Body */
   FTPd_CONTEXT               ftpd_context =  { 0 };
   sockaddr_in                laddr;
   uint_32                    sock, listensock;
   uint_32                    error=RTCS_OK;
   uint_16                    remote_addr_len;
   sockaddr_in                remote_addr = {0};
   TASK_TEMPLATE_STRUCT_PTR   t_ptr;
   FTPd_SESSION_PTR           session_ptr;
   uint_32                    option;
   boolean                    dev_in_path = FALSE;
   int_16                     devlen = 0, rootdirlen = 0;

   FTPd_task_id = RTCS_task_getid();
#ifdef __MQX__
   /* Set up exit handler and context so that we can clean up if the FTP Server is terminated */
   _task_set_environment( _task_get_id(), (pointer) &ftpd_context );
   _task_set_exit_handler( _task_get_id(), FTPd_Exit_handler );
#endif
   t_ptr = _task_get_template_ptr(MQX_NULL_TASK_ID);

   laddr.sin_family      = AF_INET;
   laddr.sin_port        = IPPORT_FTP;
   laddr.sin_addr.s_addr = INADDR_ANY;

   /* Listen on TCP port */
   ftpd_context.LISTENSOCK = socket(PF_INET, SOCK_STREAM, 0);
   listensock = ftpd_context.LISTENSOCK;
   if (listensock == RTCS_SOCKET_ERROR) {
      error = RTCSERR_OUT_OF_SOCKETS;
   }
  
   if (!error) {
      option = FTPd_window_size;  
      error = setsockopt(listensock, SOL_TCP, OPT_TBSIZE, &option, sizeof(option));
   }
  
   if (!error) {
      option = FTPd_window_size;  
      error = setsockopt(listensock, SOL_TCP, OPT_RBSIZE, &option, sizeof(option));
   }     

   if (!error) {
      option = FTPDCFG_SEND_TIMEOUT;  
      error = setsockopt(listensock, SOL_TCP, OPT_SEND_TIMEOUT, &option, sizeof(option));
   }  

   if (!error) {
      option = FTPDCFG_CONNECT_TIMEOUT;  
      error = setsockopt(listensock, SOL_TCP, OPT_CONNECT_TIMEOUT, &option, sizeof(option));
   }  

   if (!error) {
      option = FTPDCFG_TIMEWAIT_TIMEOUT;  
      error = setsockopt(listensock, SOL_TCP, OPT_TIMEWAIT_TIMEOUT, &option, sizeof(option));
   }  

   if (!error) {
      error = bind(listensock, &laddr, sizeof(laddr));
   }

   if (!error) {
      error = listen(listensock, 0);
   }

   if (error) {
      RTCS_task_exit(creator, error);
   }
   RTCS_task_resume_creator(creator, RTCS_OK);

   for (;;) {

      /* Connection requested; accept it */
      remote_addr_len = sizeof(remote_addr);
      sock = accept(listensock, &remote_addr, &remote_addr_len);
     
      if ((sock != 0) && (sock!=RTCS_SOCKET_ERROR)) {
         session_ptr = (FTPd_SESSION_PTR) RTCS_mem_alloc_zero(sizeof (FTPd_SESSION_STRUCT));

         if ( session_ptr ) {
            _mem_set_type(session_ptr, MEM_TYPE_FTPd_SESSION_PTR);

            session_ptr->DATA_BUFFER_SIZE = FTPd_buffer_size;
            session_ptr->DATA_BUFFER_PTR = RTCS_mem_alloc_zero(session_ptr->DATA_BUFFER_SIZE);
            if (session_ptr->DATA_BUFFER_PTR == NULL) {
               _mem_free(session_ptr);
               session_ptr = NULL;
            } else {
               _mem_set_type(session_ptr->DATA_BUFFER_PTR, MEM_TYPE_FTPd_DATA_BUFFER);
            }
         }
           
           
         if (session_ptr == NULL) {
            shutdown((uint_32)sock, FTPDCFG_SHUTDOWN_OPTION);
         } else  {
     

            session_ptr->CONTROL_SOCK = (uint_32) sock;
            session_ptr->CONNECTED = TRUE;
            /* set default data ports */
            session_ptr->SERVER_DATA_SOCKADDR.sin_family      = AF_INET;
            session_ptr->SERVER_DATA_SOCKADDR.sin_port        = IPPORT_FTPDATA;
            session_ptr->SERVER_DATA_SOCKADDR.sin_addr.s_addr = INADDR_ANY;

            session_ptr->USER_DATA_SOCKADDR.sin_family      = remote_addr.sin_family;
            session_ptr->USER_DATA_SOCKADDR.sin_port        = remote_addr.sin_port;
            session_ptr->USER_DATA_SOCKADDR.sin_addr.s_addr = remote_addr.sin_addr.s_addr;

#if FTPDCFG_USES_MFS
            //initialize current directory and current filesystem
            devlen = _io_get_dev_for_path(session_ptr->CURRENT_FS_NAME,
                        &dev_in_path,
                        FTPD_DEVLEN,
                        (char *)FTPd_rootdir,
                        NULL);
                       
            session_ptr->CURRENT_FS = _io_get_fs_by_name(session_ptr->CURRENT_FS_NAME);
           
            error = ioctl(session_ptr->CURRENT_FS, IO_IOCTL_CHECK_DIR_EXIST,(pointer)FTPd_rootdir ); 
           
            if (error)  {
#endif           
               session_ptr->CURRENT_FS = NULL;
               session_ptr->CURRENT_FTP_DIR = NULL;
               session_ptr->CURRENT_FS_DIR[0] = '\0';
#if FTPDCFG_USES_MFS              
            } else {
               // set current fs dir (including root dir)
               strcpy(session_ptr->CURRENT_FS_DIR,FTPd_rootdir+devlen);
              
               rootdirlen = strlen(session_ptr->CURRENT_FS_DIR);

               // set current FTP dir
               session_ptr->CURRENT_FTP_DIR = session_ptr->CURRENT_FS_DIR + rootdirlen - 1;
              
               //check if there is / at the end of root dir name
               if(*(session_ptr->CURRENT_FTP_DIR) != '\\' &&
                  *(session_ptr->CURRENT_FTP_DIR) != '/')
               {
                  session_ptr->CURRENT_FTP_DIR++;
               }
             session_ptr->CURRENT_FTP_DIR[0] = '\\';
             session_ptr->CURRENT_FTP_DIR[1] = '\0';
            }
#endif                    
            #if FTPDCFG_ENABLE_MULTIPLE_CLIENTS
               /* Create a task to look after it */
               RTCS_detachsock(sock);
               if (RTCS_task_create("FTPd_child", t_ptr->TASK_PRIORITY, t_ptr->TASK_STACKSIZE, FTPd_child, (pointer) session_ptr) != RTCS_OK ) {
                  RTCS_attachsock(sock);
                  shutdown(sock, FLAG_ABORT_CONNECTION);
                  _mem_free(session_ptr->DATA_BUFFER_PTR);
                  _mem_free(session_ptr);
            #else
               FTPd_child((pointer) session_ptr,0);
            #endif

         }        
      }
   }
}

 

 

 

 PetrL

 

 

0 Kudos
Reply
1,989 Views
gmabey
Contributor I
Thank you, PetrL.  
0 Kudos
Reply