MFS shell commands and multiple MFS file systems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFS shell commands and multiple MFS file systems

Jump to solution
3,543 Views
pbanta
Contributor IV

With MQX 3.8.1 on a K70 I have two MFS filesystems created in this order:

1.  a: is installed on a RAM disk

2.  c: is installed on an SD card

Through a telnet shell I'm trying to use the MFS shell commands to test file creation/read/write/delete on the SD card.  The only command that seems to recognize the c: filesystem is df.  Other commands, like "create" and "dir" seem to only work with the first file system they find. See the shell output below.

shell> df a:

Free disk space on a:

2033 clusters, 512 bytes each

1016 KB

shell> df b

Error, file system not mounted

shell> df c:

Free disk space on c:

975594 clusters, 4096 bytes each

3902376 KB

shell> create a:test.txt

Error, unable to open file a:test.txt.

shell> create c:test.txt

Error, unable to open file c:test.txt.

shell> create test.txt

shell> dir

TEST.TXT            0 01-01-1980 00:03:16      A TEST.TXT

shell> dir a:

shell> dir c:

shell>

A little background:

I have partitioned and formatted the SD card with MQX/MFS.  I know that in my SD card init function I can create a file successfully.  I can then put the card in a PC and see the file I created.  It's just that from the MQX shell that not all of the MFS shell commands seem to work.  I must have something mis-configured. 

Any ideas?

Paul


Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,366 Views
BryGuyH
Contributor IV

The shell functions don't accept absolute paths. Change directories first using cd to the root directory of the drive you're interested in.

View solution in original post

0 Kudos
Reply
4 Replies
2,367 Views
BryGuyH
Contributor IV

The shell functions don't accept absolute paths. Change directories first using cd to the root directory of the drive you're interested in.

0 Kudos
Reply
2,365 Views
pbanta
Contributor IV

Bingo.  Thank you so much.

Maybe I spoke too soon...

I can change directory and see files on the SD card using "dir", but I still can't create files.  The file system can't be read-only because I can create a file during the init, but not later.

Message was edited by: Paul Banta

0 Kudos
Reply
2,365 Views
BryGuyH
Contributor IV

Try to copy or compare two files on the drive to see if at least you can read from it.

0 Kudos
Reply
2,365 Views
pbanta
Contributor IV

I can't read from a file.  I put an s-record file on the SD card using the card reader attached to my PC.  I tried the "type" command to dump the file and my board crashed.  I'll keep looking.

0 Kudos
Reply