Hello,
I would like to update this thread, since MQX 4.0 release notes state the following:
<<
Ready for new Freescale NAND Flash File System library.
o The MQX 4.0 has been tested with the new FFS library which implements the wear leveling algorithms and support for on-chip NAND Flash controller.
o This library enables the MFS filesystem to be installed and used on top of the NAND Flash memory devices.
o The FFS library is available as a standalone installation package.
>>
Unfortunately, I was not able to find any link to a so-called "Freescale NAND Flash File System library". All I could find where links to third-party commercial solutions.