MFS on SD card cannot create files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFS on SD card cannot create files

1,044 Views
mscovel
Contributor III

Following the sdcard example, I am able to read files on the SD card on tower K65. Thanks for the help everyone!

But I find that I can't create new files on the SD card. I step through the fopen code and can see that it recognizes that the file does not exist but it just gives up. 

esdhc and sdcard are installed.I have verified that the partition manager is mounted. a: is opened.

What am I missing?

0 Kudos
Reply
2 Replies

901 Views
mscovel
Contributor III

It was my fault. Stack overflow. MFS works very well.

0 Kudos
Reply

901 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Mark:

How can I reproduce your issue in my side

Also please check whether the sdcard write-protected?

Regards

Daniel

0 Kudos
Reply