MQX mfs in KSDK 1.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX mfs in KSDK 1.3

1,581 Views
mscovel
Contributor III

I'm trying to understand how to get MFS/nio to work on an SDHC card in KSDK1.3 (twrk65f180m) in KDS3.2.

I've run the sdcard example which runs but does not seem to recognize commands nor do anything useful.

I've linked in RTCS.

What do I have to do to get MFS started?

What do I have to do to get MFS writing files to the SD card?

What do I have to do to use the MFS API to write files from code/tasks?

4 Replies

1,255 Views
mscovel
Contributor III

After following the doc above and others as well as the excellent examples, I was able to get RTCS, FTP and MFS running. Kudos to Freescale for making strong software enablement free. I am impressed.

0 Kudos
Reply

1,255 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Mark:

Please kindly refer to the below document for add MFS to a MQX RTOS for KSDK project.

https://community.nxp.com/docs/DOC-233598

I hope it is helpful.

Regards

Daniel

0 Kudos
Reply

1,255 Views
mscovel
Contributor III

document you posted isn't there

Thanks

Mark Scovel

260-515-2491

On Fri, Dec 1, 2017 at 12:40 AM, danielchen@fsl <admin@community.nxp.com>

0 Kudos
Reply

1,255 Views
danielchen
NXP TechSupport
NXP TechSupport

Sorry , maybe a typo, please try this link.

https://community.nxp.com/docs/DOC-233598