MFS at internal flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFS at internal flash

Jump to solution
2,471 Views
Tgomes
Contributor III

Hi,

 

 

Is there a simple way to use the internal flash to store and manipulate files by using MFS? If so, it is possible to know or configure how much space I have available?

 

 

Regards,

Tgomes.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,852 Views
Tgomes
Contributor III

Resolved (in another way)

I decided to work with the file system on a sdcard, available on my board. Now I have enough space to save my files and create folders.

 

 

Thanks for help!

View solution in original post

0 Kudos
Reply
3 Replies
1,852 Views
timias
Contributor IV

Did you look at the RAM Disk Example?

0 Kudos
Reply
1,852 Views
Tgomes
Contributor III
Timias, Yes, but use the MFS in RAM would not be appropriate for my project. Thank you for answering! Att.
0 Kudos
Reply
1,853 Views
Tgomes
Contributor III

Resolved (in another way)

I decided to work with the file system on a sdcard, available on my board. Now I have enough space to save my files and create folders.

 

 

Thanks for help!

0 Kudos
Reply