MFS at internal flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFS at internal flash

ソリューションへジャンプ
2,466件の閲覧回数
Tgomes
Contributor III

Hi,

 

 

Is there a simple way to use the internal flash to store and manipulate files by using MFS? If so, it is possible to know or configure how much space I have available?

 

 

Regards,

Tgomes.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,847件の閲覧回数
Tgomes
Contributor III

Resolved (in another way)

I decided to work with the file system on a sdcard, available on my board. Now I have enough space to save my files and create folders.

 

 

Thanks for help!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,847件の閲覧回数
timias
Contributor IV

Did you look at the RAM Disk Example?

0 件の賞賛
返信
1,847件の閲覧回数
Tgomes
Contributor III
Timias, Yes, but use the MFS in RAM would not be appropriate for my project. Thank you for answering! Att.
0 件の賞賛
返信
1,848件の閲覧回数
Tgomes
Contributor III

Resolved (in another way)

I decided to work with the file system on a sdcard, available on my board. Now I have enough space to save my files and create folders.

 

 

Thanks for help!

0 件の賞賛
返信