MFS SDHC Class 4 on K70 Tower Throughput

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFS SDHC Class 4 on K70 Tower Throughput

1,491件の閲覧回数
fanl
Contributor I

Hello.

 

I have ran some experiments on the TWR board and achieved 1.3MB/s of write performance on a SDHC Class 4 of 4GB. The experiment was run from a task inside of the MQX RTOS. 

 

Whould you have any performance measurements made on other Freescale's MCU or even on Kinetis as well?

 

If you have any ideas of how to increase the write performance, please, tell me. My application requires 2MB/s of performance.

 

Att.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,226件の閲覧回数
pavel_chromy
NXP Employee
NXP Employee

Hello,

recently there was extensive performance optimization in MFS and SDCARD/ESDHC drivers, however these changes are not part of upcomming 3.8.1 yet, this is planned to appear in the next release. I belive that 2 MB/s should be achievable with the optimized MFS and drivers.

Regards, Pavel