MCG_ATC undefined in BSP_CM.c using MQX 4.1.1 and IAR 7.30.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCG_ATC undefined in BSP_CM.c using MQX 4.1.1 and IAR 7.30.1

919 Views
jlag
Contributor II

Compiling the libs for TWRK60D512 and many undefined symbols in BSP_CM.c.

This is clean fresh install of MQX and IAR. TWRK60D100M builds fine.

Has anyone else experienced this?

Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 205

Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 208

Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 210

Error[Pe020]: identifier "MCG_ATC_ATME_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 210

Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 212

Error[Pe020]: identifier "MCG_ATC_ATMF_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 212

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 349

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 389

Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 403

Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 422

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 450

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 514

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 551

Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 820

Error[Pe020]: identifier "MC_PMCTRL" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 836

Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 913

Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 952

Error[Pe020]: identifier "LLWU_CS" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 1021

0 Kudos
Reply
1 Reply

687 Views
soledad
NXP Employee
NXP Employee

Hi John,

Unfortunately I cannot to reproduce your issue. I am using MQX4.1.1 and IAR 7.1.

According with the release notes, Freescale MQX RTOS was compiled and tested with IAR Embedded Workbench® for ARM® Version 7.10.3.

Did you try using IAR 7.10??


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply