MCF54418 Use 8bit NAND flash still failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54418 Use 8bit NAND flash still failed

742 Views
eric_wu
Contributor I

     We now use a board based on MCF54418,and its circuit is the same as development board(TWR-MCF5441x (700-26131))bought from freescale。The NAND flash is 16bit IC MT29F2G16AADWP . But now,we want change NAND flash to 8bit MT29F2G08ABAEAWP‐IT because of its lifecycle.

     About the code , i have just change "#define MT29F2G16_WIDTH                   16" to "8" in MT29F2G16.c as below. But it does not work.

     So I am very confused for a long time. Is there anything else should be change?

19290_19290.png001.PNG.png

0 Kudos
Reply
1 Reply

641 Views
soledad
NXP Employee
NXP Employee

Hello Eric,

Please check my answer in the thread Re: MCF54418 Use 8bit NAND flash failed

and let me know if this helps!!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply