MCF5225x MQX3.6 MFS IO_IOCTL_FIND_FIRST_FILE problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5225x MQX3.6 MFS IO_IOCTL_FIND_FIRST_FILE problem

1,783 次查看
ARQuattr
Contributor IV

I'm running MFS and USB host MSD stack to read files from a USB drive.  The drive is mounted fine and in the shell prompt I can enter dir and get a directory listing.  All the other MFS shell commands seem to work normally as well.  But I also have some code that attempts to get the first file from the directory but it returns -1.  The code is essentially the same as the example given in the MFS user guide (rev2.2, page 32), so I'm not sure what's wrong.  I also don't recognize that error code (-1).  I would expected an error to be positive and in the 0x3000 range.

_mqx_int error_code;

MFS_SEARCH_DATA search_data;

MFS_SEARCH_PARAM search;

char filepath[] = “*.*”;

search.ATTRIBUTE = MFS_SEARCH_ANY;

search.WILDCARD = filepath;

search.SEARCH_DATA_PTR = &search_data;

error_code = ioctl(mfs_fd_ptr, IO_IOCTL_FIND_FIRST_FILE,(uint_32_ptr) &search);

while (error_code == MFS_NO_ERROR) {

     printf ("%-12.12s\n", search_data.NAME);

     error_code = ioctl(mfs_fd_ptr, IO_IOCTL_FIND_NEXT_FILE, (uint_32_ptr) &search_data);

} else {

     printf ("error code %d\n", error_code);

}

Output:

error code -1

Any advice on what might be the problem, or what I could try to fix it?

Thank you

标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

1,452 次查看
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Angelo,

I wrote this code some months ago. I believe it is still working. Please, try it and share your results:

pastedImage_0.png

/******************************************************/

int_32 test_find(int_32 argc, char_ptr argv[] )

{

_mqx_int error_code = MFS_NO_ERROR;

MFS_SEARCH_DATA search_data;

MFS_SEARCH_PARAM search;

char filepath [6]= "a:\\*.*";

MQX_FILE_PTR fs_ptr = NULL;

fs_ptr = _io_get_fs_by_name("a:");

search.ATTRIBUTE = MFS_SEARCH_ANY;

search.WILDCARD = (char_ptr)&filepath;

search.SEARCH_DATA_PTR = &search_data;

error_code = ioctl(fs_ptr, IO_IOCTL_FIND_FIRST_FILE, (uint_32_ptr) &search);

while (error_code == MFS_NO_ERROR)

{

printf ("%-12.12s %6lu %02lu-%02lu-%04lu %02lu:%02lu:%02lu\n",

search_data.NAME,

search_data.FILE_SIZE,

(uint_32)(search_data.DATE & MFS_MASK_MONTH)   >>MFS_SHIFT_MONTH,

(uint_32)(search_data.DATE & MFS_MASK_DAY)     >>MFS_SHIFT_DAY,

            (uint_32)((search_data.DATE & MFS_MASK_YEAR)   >>MFS_SHIFT_YEAR) + 1980,

            (uint_32)(search_data.TIME & MFS_MASK_HOURS)   >>MFS_SHIFT_HOURS,

            (uint_32)(search_data.TIME & MFS_MASK_MINUTES) >>MFS_SHIFT_MINUTES,

            (uint_32)(search_data.TIME & MFS_MASK_SECONDS) <<   1);

error_code = ioctl(fs_ptr, IO_IOCTL_FIND_NEXT_FILE,(uint_32_ptr) &search_data);

}

return error_code;

}

/******************************************************/

Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,452 次查看
maddyv
Contributor I

We are facing the same problem. Any advice on what might be the problem.

Thanks,

Maddy

0 项奖励
回复