MCF51CN MQX application + FNET bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF51CN MQX application + FNET bootloader

653 次查看
butok
NXP Employee
NXP Employee

If you have an issue to run MQX + FNET Bootloader on Lasco.

 

You should aply workaround to MQX code (otherwise it goes to infinite “while” )

      /Special thanks to Amly/


bsp_init.c (for mcf51cn platform):

 

static void _mqx_clock_init_25MHz()

{

   ...............................................

#if 0  

   //b) Loop until OSCINIT (bit 1) in MCGSC is 1, indicating the crystal selected by the EREFS bit

   //has been initialized.

   while (!(reg_ptr->MCG.MCGSC & MCF51XX_MCGSC_OSCINIT_MASK))     

   ;

#endif  

   ...............................................

  

#if 0

   // wait for Reference Status bit to update

   while (!(reg_ptr->MCG.MCGSC & MCF51XX_MCGSC_IREFST_MASK))

   ;

#endif

   ...............................................

 

}

Hope it be fixed in the future version of MQX.

 

 

Also the standard modifications that are valid for all platforms:

 

1. user_config.h

#define MQX_ROM_VECTORS                0

 

2. intflash_FNET.lcf

MEMORY

{


    fnet_bootloader  (RX)  : ORIGIN = 0x00000000, LENGTH = 0x0000B000 # 44KB reserved for FNET bootloader

#   cfmprotrom       (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000020 

    vectorrom        (RX)  : ORIGIN = 0x0000B000, LENGTH = 0x00000400

#   rom              (RX)  : ORIGIN = 0x00000420, LENGTH = 0x0001FBDF  # Code + Const data

    rom              (RX)  : ORIGIN = 0x0000B400, LENGTH = 0x00014800  # Code + Const data

    fapp_paramsrom   (RW)  : ORIGIN = 0x0001FC00, LENGTH = 0x00000400 # 1KB = Last logical-block resevrd for params.

    ram             (RWX)  : ORIGIN = 0x00800000, LENGTH = 0x00006000  # SRAM - RW data

 

   # kernel space starts after RAM variables (Location of MQX Kernel data + MQX heap)

   end_of_kd   (RW): ORIGIN = 0x00805FF0, LENGTH = 0x00000000

  

   # Boot stack reused by MQX Kernel data

   bstack      (RW): ORIGIN = 0x00805A00, LENGTH = 0x00000200  # Boot stack

   end_bstack  (RW): ORIGIN = 0x00805BFF, LENGTH = 0x00000000

}

 

SECTIONS

{

  ........................

                #.cfmprotect :

                #{

                #             *(.cfmconfig)

                #             . = ALIGN (0x4);

                #} > cfmprotrom

  .........................

}

 

 

Best regards,

Andrey Butok

0 项奖励
回复
0 回复数