Looking for a DNS client / DHCP client example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for a DNS client / DHCP client example

ソリューションへジャンプ
7,348件の閲覧回数
vier_kuifjes
Senior Contributor I

I have a Coldfire Lite based application that I would like to try to port to MQX. This application works as a HTTP client (not a HTTP server as in most demo apps).

 

There is a lot of MQX documentation available, which I'm reading, but some practical examples are sometimes more useful. Can someone provide me with some working code examples of a DHCP client and DNS client?

 

Any help is much appreciated!

ラベル(1)
タグ(1)
1 解決策
3,701件の閲覧回数
EAI
Contributor IV
Many of the examples provided in the releaseare configured with DHCP and DNS clients. You can look at demo\security_email\security_network.c as one example.

元の投稿で解決策を見る

5 返答(返信)
3,702件の閲覧回数
EAI
Contributor IV
Many of the examples provided in the releaseare configured with DHCP and DNS clients. You can look at demo\security_email\security_network.c as one example.
3,701件の閲覧回数
AloysiusJegan
Contributor III

Thanks for the info. I implemented in my project and it is working fine.

 

 

Regards

Aloysius Jegan

 

http://www.aloysiusjegan.in

 

 

 

0 件の賞賛
返信
3,701件の閲覧回数
vier_kuifjes
Senior Contributor I

Thanks.

 

Is this file actually being used in any of the demo projects? There doesn't appear to be a .mcp file  in the security_* folders...

0 件の賞賛
返信
3,701件の閲覧回数
vier_kuifjes
Senior Contributor I
Anyone?
0 件の賞賛
返信
3,701件の閲覧回数
AloysiusJegan
Contributor III

Anyone?????????

Even I also want the same...

 

 

-AJ

 

http://www.aloysiusjegan.in

0 件の賞賛
返信