Linker / Compilier Auto aligh uint_32's?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker / Compilier Auto aligh uint_32's?

ソリューションへジャンプ
2,846件の閲覧回数
CarlFST60L
Senior Contributor II

Hi,

 

MQX3.6.2 + CW7.2+MCF52259evb

 

I have the following C file

 

 

in envm.c#include <ctype.h>#include <mqx.h>#include <bsp.h>#include "envm.h"#pragma explicit_zero_data on#pragma force_active onvolatile uint_32 TEST1 = 1;         //This is a specific random number defined in the headervolatile uchar TEST2 = 0;volatile uint_32 TEST3 = 2;         //This is a specific random number defined in the headervolatile uchar TEST4 = 4;        //Compile Time#pragma explicit_zero_data off#pragma force_active off

 

In my linker, I added the following twoENVM_DATA   (RW): ORIGIN = 0x10050000, LENGTH = 0x00001000  # MRAM space for some dataand .ENVM_DATA_Page: {  envm.c (.data)  envm.c (.rodata)  envm.c (.text) } > ENVM_DATA

 

In xMAP output I get the following:

 

 

# .ENVM_DATA_Page
  10050000 00000004 .data   TEST1    (envm.c)
  10050004 00000001 .data   TEST2    (envm.c)
  10050008 00000004 .data   TEST3    (envm.c)
  1005000C 00000001 .data   TEST4    (envm.c)

 

I want to understand why TEST3 is aligned at 10050008 instead of 10050005

 

I have tried adding the following in my linker, the results were the same

 

. = ALIGN (0x1);

 

Is there a reason for this? Is it normal? Can I force them to be 'one after the other' and still work as expected?

 

 

0 件の賞賛
返信
1 解決策
2,454件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi Carl,

 

what you see is normal behaviour of compiler, where all 32-bit value is aligned. That's because of bus access optimization.

You can use #pragma align as the compiler directive to change default alignement of a variable.


元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,455件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi Carl,

 

what you see is normal behaviour of compiler, where all 32-bit value is aligned. That's because of bus access optimization.

You can use #pragma align as the compiler directive to change default alignement of a variable.


0 件の賞賛
返信
2,454件の閲覧回数
CarlFST60L
Senior Contributor II

Thanks for the reply,

 

I would have though that . = ALIGN (0x01); would have worked.

 

Thanks again, we ended up using a slightly different techniques to get around the issue we were having.

 

Thanks again,

Carl

0 件の賞賛
返信
2,454件の閲覧回数
JuroV
NXP Employee
NXP Employee

You know, accessing unaligned variables can have impact not only to linker, but also to compiler- depends on architecture (getting each byte and assembling a 32bit value). That's why the #pragma is used during compilation time.

2,454件の閲覧回数
CarlFST60L
Senior Contributor II

That makes sense, thanks JuroV! 

0 件の賞賛
返信