KwikStik Patch for 3.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KwikStik Patch for 3.7

1,485件の閲覧回数
BenG
Contributor III

I've just installed MQX 3.7 and then attempted to install the Kwik Stick Patch for 3.7 (FSLMQXOS_3_7_0_KwikStik_Patch.exe).

 

This patch doesn't allow me or ask me where I want to install the patch. If I've got multiple installations of MQX on my Hard Drive, it's kind of Pot Luck which folder/Installation the patch install to. Is there a way to chose a directory/folder when installing this patch.

 

(As an aside - I'm currently download MQX 3.8 so I'm assuming/hoping I won't need to install the patch for 3.8 as I understand BSP support for Kwik Stick is included by default in the 3.8 download)

0 件の賞賛
返信
2 返答(返信)

1,351件の閲覧回数
c0170
Senior Contributor III

Hi BenG,

 

kwikstik is supported in MQX 3.8 . Any patch is not needed.

 

Back to the patch for 3.7. I assume it's bound to the MQX_ROOT , I'll let you know if otherwise.

 

Regards,

MartinK

0 件の賞賛
返信

1,351件の閲覧回数
BenG
Contributor III

Cheers,

 

3.8 Downloaded overnight so I'm goign to gave that a go today.

0 件の賞賛
返信