KDS with MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS with MQX

6,391 次查看
garimaparashar
Contributor III

Hi,

I am working with CodeWarrior and of MQX 4.0

Now I need to move on KDS. For that I installed KDS and Kinstis SDK. Also installed MQX 4.2.

What problem I am facing is, I made my project with CodeWarrior v10.6 and with MQX v4.0.

And Now I want to move towards KDS.

So when I have imported MQX 4.2 project (hello demo example), It is showing me an error that "undefined mqx.h" .

I don't understand what is wrong with it.

What kind of Change i need to made? So that I can directly import my previous project. Or can access my previous source code files.

Is there any steps that I need to follow?

Regards,

Garima Parashar

标记 (1)
0 项奖励
回复
4 回复数

6,085 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Garima Parashar.

please check if this document can help you.

Importing MCU V10.6 projects (sample, using PE and MQX) under KDS


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,084 次查看
garimaparashar
Contributor III

Hi Zhang,

Thanx for the information.

I am following a "Creating a New MQX RTOS for KSDK1.2 Project in KDS3.0.pdf" (Attaching with this mail) . I followed it and uptill point 3.19 there is no problem I am facing.

But on point 4. when I am buiding a project that show me an error " fatal error: psptypes.h: No such file or directory". I dont know why this is happening??

Also one more thing.,

3.12 Go to menu Project > Properties > C/C++ Build > Settings > Cross ARM C++ Linker >

Miscellaneous and add all the Libraries with their full paths. (I am working on TWR-K60D100M)

the paths to be replaced are.,

C:\Freescale\KSDK_1.2.0\lib\ksdk_mqx_lib\kds\K60D10\debug\libksdk_platform_mqx.a

C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\twrk60d100m.kds\debug\mqx_stdlib\lib_mqx_stdlib.a

C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\twrk60d100m.kds\debug\mqx\lib_mqx.a

but when I go to this path, I found that lib_mqx_stdlib.a and lib_mqx.a are not available there..!!

I don't know what to do?

Please help me to sort this out

Regards,

Garima

0 项奖励
回复

6,084 次查看
garimaparashar
Contributor III

Hi Zhang,

Somehow I tried to remove the errors and Now my project is error free.

But What I am seeing.,

When I tried to run project (By right click on project and Run) that show me an error (Attached with this mail).

Same case when I tried to debug by right click on project and Debug. (Error Attached with this mail).

Now when I am debugging a project by go to Debug Configuration->Select GDB PEMicro Interface Debug-> Debug then it will not show me an error and debugs well., I don't understand what I need to do now.

Can you please suggest me any further settings for Run and Debug Configuration.

Regards,

Garima

0 项奖励
回复

6,084 次查看
soledad
NXP Employee
NXP Employee

Hello Garima,

Please check the below document and let me know if this helps,

Creating a New MQX RTOS 4.2 project in KDS


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复