K70 Ethernet usage.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K70 Ethernet usage.

800 次查看
sudhanshumehta
Contributor IV


Hi team,

I am having TWR-K70F120M and TWR-SER modules.

TWR-K70F120M  module has SCH-27166 Rev C2

I am working for Ethernet communication (RTCS).

I want to get verified following things.

Jumper connections of TWR-K70F120M.

          J18 is OFF     and J19 is ON.

   Jumper connections of TWR-SER.

                 J2--> 3-4 is ON (pin 3-4 are short),            J12 --> 9-10 is ON,                     J3-->2-3 is ON.

I will use MQX 4.2.

Additionally I will use "eth_to_serial" example given at "C:\Freescale\Freescale_MQX_4_2\rtcs\examples".

Kindly verify the bold items.

Thanks

Sudhanshu

0 项奖励
回复
1 回复

598 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Check C:\Freescale\Freescale_MQX_4_2\doc\ MQX_Getting_Started.pdf

image001.png

Luis

0 项奖励
回复