K64 Freedom _task_delay() not Working Properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 Freedom _task_delay() not Working Properly

4,642 Views
razed11
Contributor V

The BSP documentations says: ...Alternatively, the bsp_cm.c can be modified manually without PEx.

It then goes on to say nothing more about it. A document about changing clock settings is referenced but I can't find it anywhere.

I'd like to understand how the clocks are configured. I'm wondering how SysTick is configured because on the K64 Freedom when I call _task_delay(10) I'm getting 150 ms instead.

Tags (2)
0 Kudos
Reply
2 Replies

4,498 Views
soledad
NXP Employee
NXP Employee

Hi Kenny,

I am attaching this document, this document is located at the path: C:\Freescale\Freescale_MQX_4_1\doc\tools\cw


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,498 Views
razed11
Contributor V

Thanks! A little bias towards the CW people I see. Let me see if this helps.

0 Kudos
Reply