K40 MQX SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,813件の閲覧回数
edsonsanchez
Contributor I

Hi,

I am working with the K40 tower and was able to build and debug the example SPI project in the MQX directory. I realize that this example is supposed to transfer data to an external memory device. I was hoping I would be able to see at least a clock signal on one of the SPI pins, but I don't. Am I supposed to see anything or do I have to do something before I can actually see a clock signal?

I was also hoping to be able to use this example project to later change the data sent out and the device I send to. Where would I make these changes?

Thanks!

Edson

0 件の賞賛
返信
1 解決策
1,724件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Edson,

you dont need special settings to see SPI clock. I was able to see this signal in oscilloscope, you can use the side expansion port connectors in the external side of TWR-ELEVATOR, many pins are mapped here. You can check the port number where each pinn is mapped in the TWR-K40 schematic, in this case SPI0_SCK is mapped to port B15 and SPI1_SCK to B7.

Hope this helps,

Carlos

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,725件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Edson,

you dont need special settings to see SPI clock. I was able to see this signal in oscilloscope, you can use the side expansion port connectors in the external side of TWR-ELEVATOR, many pins are mapped here. You can check the port number where each pinn is mapped in the TWR-K40 schematic, in this case SPI0_SCK is mapped to port B15 and SPI1_SCK to B7.

Hope this helps,

Carlos

0 件の賞賛
返信
1,724件の閲覧回数
edsonsanchez
Contributor I

Thanks Carlos! I can see the clock signal. Any idea how I can change the pin mapping? Also, do you know which part of the code I should modify to get a different set of data out of the MOSI pin?

Edson

0 件の賞賛
返信