K10DN512 .icf file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10DN512 .icf file

Jump to solution
2,361 Views
albertnguyen
Contributor II

Does anyone have the K10DN512 .icf file? I want to make sure mine match up. 

I keep getting this warning/error    Stack pointer is setup to incorrect alignment. Stack addr = 0x1FFFFEFF    whenever I do a download/debug

0 Kudos
Reply
1 Solution
2,167 Views
albertnguyen
Contributor II

I redid the port with BSP cloning wizard. Didn't need to touch the icf file anymore. It is working now.

View solution in original post

0 Kudos
Reply
3 Replies
2,168 Views
albertnguyen
Contributor II

I redid the port with BSP cloning wizard. Didn't need to touch the icf file anymore. It is working now.

0 Kudos
Reply
2,167 Views
albertnguyen
Contributor II

Attached is the one I currently have.

0 Kudos
Reply
2,167 Views
soledad
NXP Employee
NXP Employee

Hello Albert,

Could you please try using the attached file?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply