K10DN512 .icf file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,364件の閲覧回数
albertnguyen
Contributor II

Does anyone have the K10DN512 .icf file? I want to make sure mine match up. 

I keep getting this warning/error    Stack pointer is setup to incorrect alignment. Stack addr = 0x1FFFFEFF    whenever I do a download/debug

0 件の賞賛
返信
1 解決策
2,170件の閲覧回数
albertnguyen
Contributor II

I redid the port with BSP cloning wizard. Didn't need to touch the icf file anymore. It is working now.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,171件の閲覧回数
albertnguyen
Contributor II

I redid the port with BSP cloning wizard. Didn't need to touch the icf file anymore. It is working now.

0 件の賞賛
返信
2,170件の閲覧回数
albertnguyen
Contributor II

Attached is the one I currently have.

0 件の賞賛
返信
2,170件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Albert,

Could you please try using the attached file?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信