K-70 USB Device CDC virtual com port stop sending data when stressed in full duplex mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K-70 USB Device CDC virtual com port stop sending data when stressed in full duplex mode.

1,045 Views
poul-erikhansen
Contributor II

I am using the MQX 4.1 and the associated USB device stack. I am using the IAR compiler.

I make a virtual COM port on the device, and when I communicate in half duplex (sending 4096 bytes from Windows 7 to the device, and waiting for the device to echo back the same 4096 bytes) every thing works fine. If I start echo back data once they are received the stack stop sending data after some time. I can remove the USB connection and reconnect but the connection from the device to the host will still be blocked.


Does anyone have any suggestions?


Poul-Erik.


Tags (1)
0 Kudos
Reply
0 Replies