Issue with DAC with DMA and PDB using PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with DAC with DMA and PDB using PE

1,575件の閲覧回数
anniepaul
Contributor II

Hello,

 

I tried to port the DAC_ADC application in K20d72m of "CW MCU v10.5\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M" to K60D100m to generate the DAC signals for playing audio. I am using PE generated code along with MQX 4.0

But I was not able to get any output in DAC0.

Please find attached the PE generated code for the above.

Kindly help me to sort out the issue. The code warrior version I am using is 10.5

 

Regards

Annie

0 件の賞賛
返信
1 返信

1,232件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Annie,

Please check the below threads:

Using DAC without PE

Using DAC component on K60 Tower

Regards

Soledad

0 件の賞賛
返信