Issue with DAC with DMA and PDB using PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with DAC with DMA and PDB using PE

1,577 Views
anniepaul
Contributor II

Hello,

 

I tried to port the DAC_ADC application in K20d72m of "CW MCU v10.5\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M" to K60D100m to generate the DAC signals for playing audio. I am using PE generated code along with MQX 4.0

But I was not able to get any output in DAC0.

Please find attached the PE generated code for the above.

Kindly help me to sort out the issue. The code warrior version I am using is 10.5

 

Regards

Annie

0 Kudos
Reply
1 Reply

1,234 Views
soledad
NXP Employee
NXP Employee

Hi Annie,

Please check the below threads:

Using DAC without PE

Using DAC component on K60 Tower

Regards

Soledad

0 Kudos
Reply