Is there any way to write to sdcard using the dma?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any way to write to sdcard using the dma?

14,537 Views
naftalir
Contributor III

Hi all,

 

if anyone have any exmample of fast writing to sdcard, with dma and/or with 4bit bandswidth, plz send me an source code..

 

Thank you so much!

Naftali. 

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,052 Views
naftalir
Contributor III

Can you be a little bit more specific on when the answers will be :smileyhappy:?

Thank you....

0 Kudos
Reply

1,052 Views
Monica
Senior Contributor III

Hey everyone!

Answers will arrive very soon!

Thanks for being all so patient!!!

Regards,

Monica

0 Kudos
Reply

1,052 Views
jonny
Contributor I

Did you have any luck with this?

0 Kudos
Reply

1,052 Views
naftalir
Contributor III

Nothing yet.... did you?

0 Kudos
Reply