Is there any cpp example for twrk22 board using KDS_2.0.0 and KSDK_1.1.0? where can I find it ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any cpp example for twrk22 board using KDS_2.0.0 and KSDK_1.1.0? where can I find it ?

735 Views
josephxavier
Contributor III

I need to run a cpp code on k22 board what are the steps to create a mqx project with cpp using KDS_2.0.0 and KSDK_1.1.0? can  any one share a simple cpp project k20 board?


0 Kudos
Reply
1 Reply

620 Views
soledad
NXP Employee
NXP Employee

Hello Joseph,

Please check the below thread

Is anyone building C++ apps with the KSDK 1.1.0 and MQX?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply