Is there any code that interacts with Freescale USB device examples for Builder C++?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any code that interacts with Freescale USB device examples for Builder C++?

跳至解决方案
6,139 次查看
JaimeR
Contributor III

I am looking for an example in Builder C++ that can send receive data trough HID functionality.

 

0 项奖励
回复
1 解答
4,439 次查看
fish_yu
Contributor III

This is a HID VCL component. It is a WinRAR File.

 

HIDController.rar

Message Edited by t.dowe on 2009-09-04 01:01 PM

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,440 次查看
fish_yu
Contributor III

This is a HID VCL component. It is a WinRAR File.

 

HIDController.rar

Message Edited by t.dowe on 2009-09-04 01:01 PM
0 项奖励
回复
4,439 次查看
JaimeR
Contributor III

I have not seen any details but on first sight it looks exactly what I was looking for.

Thanks.

 

Jaime

0 项奖励
回复
4,439 次查看
fish_yu
Contributor III

I know the answer of your problem. I am also a fans of RAD environment. I think that you may install a VCL for your C++ Builder. The VCL is a OpenSource code from A germany Engineer.You may download it from http://www.delphi-jedi.org/

The name of VCL is HIDController. There is a Typical AppNote about LPC2148 and HID Ports in NXP Semiconductor Web. You may download it to study. I think you may migrate them into Freescale MCF52259 EVB.

If you won't find the VCL, i can send it by Email; My emain: [email protected]

That' all. Good,LUCK,

0 项奖励
回复
4,439 次查看
JaimeR
Contributor III

I couldnt find the VCL, could you post the link?

I also sent an email to that email address you posted.

0 项奖励
回复
4,439 次查看
JuroV
NXP Employee
NXP Employee

Hi Jaime.

 

HID is a typical input device from the host point of view. Do you want to read data in Builder C++ application from HID device written in MQX?

0 项奖励
回复
4,439 次查看
JaimeR
Contributor III

I need to send information from the microcontroller to the PC, then make some processing(in the PC ) and send some data back to the microcontroller. With the examples provided by freescale, windows manage and does all the processing via HID drivers. I want to use HID drivers but I need to manipulate them in order to process the data they receive and use them to send the data I want. I figure that Freescale has made something like that in order to make tests.

Builder C++ is the compiler I am using, however, I might try to port the code (if there is any) from other language/compiler.

 

Regards,

 

Jaime

0 项奖励
回复