Is professional version of Code Warrior needed for MQX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is professional version of Code Warrior needed for MQX?

3,934 Views
rav
Contributor III

1) Yes You can compile in special edtion of CodeWarrior.

 

http://www.freescale.com/webapp/sps/site/overview.jsp?&code=MQXSWDW

Under Example applications:

Lab Tutorial Demos – Codewarrior™ Professional Edition (30-day evaluation available) is highly recommended to run the Freescale MQX MCF5225x lab tutorial software. Please note that Labs 1, 2, and 6 may run on CodeWarrior™ Special Edition (< 128K code size). 

 

2) OS Aware - Task aware debugging is only included with the Professional Version of CodeWarrior as a value added feature.

    

     TAD info: http://www.freescale.com/webapp/sps/site/overview.jsp?code=MQXTOOLS

     Also check out the documents.

 

     CW info: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DEBUG_COMPILERS&tid=mSDTds 

0 Kudos
Reply
0 Replies