Inter-processor communication (IPC) over CAN Bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inter-processor communication (IPC) over CAN Bus

ソリューションへジャンプ
2,788件の閲覧回数
amleng
Contributor IV

Is it possible to have IPC over CAN bus. In MQX Reference  manual I found _ipc_add_io_ipc_handler() can get  IO_CAN_COMPONENT as the parameter component but I didn't see any example code. In addition, #define 
IO_CAN_COMPONENT is commented in psp library.

0 件の賞賛
返信
1 解決策
2,372件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Sina,

The IPC examples we have are for serial and Ethernet.  Any hardware interface can be ported to.  We just haven't ported the IPC example code to every possible peripheral.

Hopefully our examples will allow you to port to a CAN interface.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,373件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Sina,

The IPC examples we have are for serial and Ethernet.  Any hardware interface can be ported to.  We just haven't ported the IPC example code to every possible peripheral.

Hopefully our examples will allow you to port to a CAN interface.

Regards,

David

0 件の賞賛
返信