Integrating FNET with MQX on the Tower 52259

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integrating FNET with MQX on the Tower 52259

ソリューションへジャンプ
2,369件の閲覧回数
accutime
Contributor III

Hi

 

Has anybody actually got FNET functioning with MQX ?

 

Is so would they supply infomation on the mapping file  "intflash.lcf" and a simple step by step guide of the integration

 

I am using the 52259 Tower Development System but it should be very similar for other V2 platforms

 

Thanks in Advance

 

Paul H

 

0 件の賞賛
返信
1 解決策
1,809件の閲覧回数
butok
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
1,809件の閲覧回数
accutime
Contributor III

Hi

 

Thanks for the document. (probably needs checking over for a few typos)

 

FNET working perfectly .

 

HIGHLY RECOMMENDED

 

Thanks

 

 

0 件の賞賛
返信
1,810件の閲覧回数
butok
NXP Employee
NXP Employee

Hi Paul,

 

You can look at this "unofficial" AN:

http://netcologne.dl.sourceforge.net/project/fnet/fnet/AN/FNET_and_MQX%20Rev%201.3.pdf

 

Best regards,

Andrey Butok

 

0 件の賞賛
返信