IPv6 and SCTP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,990件の閲覧回数
ThiagoMarinello
Contributor I

Is there any provision (roadmap) for support protocols: IPv6 and/or SCTP (Stream Control Transmission Protocol)?

Thank you.

 

Message Edited by Thiago Marinello on 2009-07-16 06:49 PM
ラベル(1)
タグ(1)
1 解決策
2,852件の閲覧回数
PetrL
NXP Employee
NXP Employee

Garabo is right, the MQX will support IPv6 soon.

  • The initial support of IPv6 is planned for MQX 4.0.0 (dec2012/jan2013). Initial support means in extend of legacy IPV6 ilver certification
  • During 2H2013 is planned to extend support and get the Golden IPv6 certification Logo

PetrL

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,852件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Thiago,

MQX 4.0 will support IPv6. There are no plans to add SCTP. THe MQX 4.0 will be released 2H2013.

Best Regards,

Garabo

2,852件の閲覧回数
mohwaqas12
Contributor III

It would be great to see IPv6 support in MQX . It would be wonderful to see sctp support too in mqx some day. I have worked on sctp and it does has some distinctive features over tcp and udp, specially the dual/multi homing for redundancy and streams for caring real time information.

Does MQX provide some kind of documentation on extending its network stack for users who would want to implement some other protocols that are not yet the part of mqx rtcs.

Regards

0 件の賞賛
返信
2,852件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport


Hi Muhammad,

MQX only provide API for application development. The documentation about the internal functions in the stack is not provided as that. However, all the functions inside has a descrition of what parameters receive and what is the reason of the function. That could help. The good thing is that the code is open and you can modify if you need to.

Best Regards,

Garabo

2,853件の閲覧回数
PetrL
NXP Employee
NXP Employee

Garabo is right, the MQX will support IPv6 soon.

  • The initial support of IPv6 is planned for MQX 4.0.0 (dec2012/jan2013). Initial support means in extend of legacy IPV6 ilver certification
  • During 2H2013 is planned to extend support and get the Golden IPv6 certification Logo

PetrL

0 件の賞賛
返信