IPv6 Support 4.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IPv6 Support 4.1.1

跳至解决方案
2,782 次查看
razed11
Contributor V

Hi,

I thought I'd give IPv6 a try. I'm using IAR with a Freedom K64.

I added the following to user_config.h and rebuilt everything but the linker cannot find IPv6 related calls.

#define RTCSCFG_ENABLE_IP6       1


Linking

Error[Li005]: no definition for "IP6_send" [referenced from tcp_send.o(rtcs.a)]

Error[Li005]: no definition for "ip6_if_get_by_scope_id" [referenced from tcp_send.o(rtcs.a)]

Error[Li005]: no definition for "ip6_if_get_by_addr" [referenced from tcp_send.o(rtcs.a)]

Error[Li005]: no definition for "IN6_ADDR_COPY" [referenced from sstream.o(rtcs.a)]

Error[Li005]: no definition for "ip6_if_select_src_addr" [referenced from iputil.o(rtcs.a)]

Error[Li005]: no definition for "in6addr_any" [referenced from tcp.o(rtcs.a)]

Error[Li005]: no definition for "RTCS6_if_get_addr" [referenced from ipcfg6.o(rtcs.a)]

Error[Li005]: no definition for "ip6_multicast_leave_entry" [referenced from udp.o(rtcs.a)]

Error[Li005]: no definition for "IP6E_send" [referenced from ip-e.o(rtcs.a)]

Error[Li005]: no definition for "IP6E_join" [referenced from ip-e.o(rtcs.a)]

Error[Li005]: no definition for "IP6E_leave" [referenced from ip-e.o(rtcs.a)]

Error[Li005]: no definition for "IP6E_close" [referenced from ip-e.o(rtcs.a)]

Error[Li005]: no definition for "IP6E_open" [referenced from ip-e.o(rtcs.a)]

Error[Li005]: no definition for "IP6_init" [referenced from tcpip.o(rtcs.a)]

Error[Li005]: no definition for "ICMP6_init" [referenced from tcpip.o(rtcs.a)]

Error[Li005]: no definition for "IP6_open" [referenced from tcp.o(rtcs.a)]

Error[Li005]: no definition for "RTCS6_if_get_scope_id" [referenced from tcp.o(rtcs.a)]

Error[Li005]: no definition for "ip6_multicast_find_socket_entry" [referenced from udp.o(rtcs.a)]

Error[Li005]: no definition for "ICMP6_send_error" [referenced from udp.o(rtcs.a)]

Error[Li005]: no definition for "IP6LOCAL_send" [referenced from iplocal.o(rtcs.a)]

Error[Li005]: no definition for "IP6LOCAL_open" [referenced from iplocal.o(rtcs.a)]

Error while running Linker

Build aborted.

标签 (1)
0 项奖励
回复
1 解答
2,610 次查看
Martin_
NXP Employee
NXP Employee

That is right. RTCS IPv4 is free, RTCS IPv6 is a paid add-on.

Internet Protocol version 6 (IPv6) for MQX RT|Freescale

-Martin

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,611 次查看
Martin_
NXP Employee
NXP Employee

That is right. RTCS IPv4 is free, RTCS IPv6 is a paid add-on.

Internet Protocol version 6 (IPv6) for MQX RT|Freescale

-Martin

0 项奖励
回复
2,175 次查看
marcomello95
Contributor I

How can I get this addon for MQX 4.2?

0 项奖励
回复