IPV6 Support v4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPV6 Support v4.2

Jump to solution
4,180 Views
Coacci
Contributor II

Hello!
I'm using MQX RTOS v4.2 and trying to use IPV6, but I have seen in the community that I would need to purchase a RTCS ipv6 paid addon to be able to use it. 
Is there any way to get this addon to v4.2?

I've searched there and soon after found out that there's no link to buy it. The  www.freescale.com/mqx/ipv6 says that it is only available on V5 without the need of this addon. 
But in my case is extremely necessary to be used the MQX RTOS v4.2 with this addon.

I appreciate any kind of help.

0 Kudos
Reply
1 Solution
4,169 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Coacci:

 

MQX v4.2 is no longer available and superseded by v5.  IPv6 is supported in MQX v5.  Please refer to below link for more information.

MQX™ v5 Software Solutions | NXP Semiconductors

 

If you only need IPv6 package, I would suggest contact  [email protected]

to see if they can provide this package to you.

 

Regards

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
4,169 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Coacci:

 

MQX v4.2 is no longer available and superseded by v5.  IPv6 is supported in MQX v5.  Please refer to below link for more information.

MQX™ v5 Software Solutions | NXP Semiconductors

 

If you only need IPv6 package, I would suggest contact  [email protected]

to see if they can provide this package to you.

 

Regards

Daniel

0 Kudos
Reply