I2C1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,375件の閲覧回数
leepenn
Contributor III


Hi,

     I am using the MQX 4.0 with Codewarrior for use on the K70. When I initialize I2C0 all is fine, I added the I2C1 initialization code to the BSP, see below. But when I try to initialize the I2C1 it causes an interrupt before the initialization can complete. I can initialize the I2C1 and communicate using a PE program. Could there be a part in the BSP for the twr k70 that is configuring the pins I need for I2C1 before it is called, and then causing my interrupt?

_mqx_int _bsp_i2c_io_init
(
    uint_32 dev_num
)
{

    PORT_MemMapPtr  pctl;
    SIM_MemMapPtr sim = SIM_BASE_PTR;

    switch (dev_num)
    {
        case 0:
            pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;

            pctl->PCR[18] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;
            pctl->PCR[19] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;

            sim->SCGC4 |= SIM_SCGC4_IIC2_MASK ;

            break;
        case 1: //I2C1, LP Added 7/25/13
            pctl = (PORT_MemMapPtr)PORTF_BASE_PTR;

            pctl->PCR[3] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK ; // PTF3, I2C1_SDA, LP Added 7/25/13
            pctl->PCR[2] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK; // PTF2, I2C1_SCL, LP Added 7/25/13

            sim->SCGC4 |= SIM_SCGC4_IIC2_MASK ;

            break;
        default:
            /* Do nothing if bad dev_num was selected */
            return -1;
    }
    return MQX_OK;

}

タグ(2)
0 件の賞賛
返信
1 解決策
3,038件の閲覧回数
Martin_
NXP Employee
NXP Employee

In MK70F12.h:

define SIM_SCGC4_IIC2_MASK                      SIM_SCGC4_IIC0_MASK

so you enable clock gate for I2C0 module in both case statements, but not for I2C1. To enable clock for IIC1 module in case 1:, make sure you set the IIC1 bit 7 of SIM_SCGC4 register. Writing to a peripheral module register with clock gated causes a hard fault exception.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,039件の閲覧回数
Martin_
NXP Employee
NXP Employee

In MK70F12.h:

define SIM_SCGC4_IIC2_MASK                      SIM_SCGC4_IIC0_MASK

so you enable clock gate for I2C0 module in both case statements, but not for I2C1. To enable clock for IIC1 module in case 1:, make sure you set the IIC1 bit 7 of SIM_SCGC4 register. Writing to a peripheral module register with clock gated causes a hard fault exception.

0 件の賞賛
返信
3,038件の閲覧回数
leepenn
Contributor III

Martin,

Thanks that was it! I changed to below and it works.

_mqx_int _bsp_i2c_io_init
(
    uint_32 dev_num
)
{

    PORT_MemMapPtr  pctl;
    SIM_MemMapPtr sim = SIM_BASE_PTR;

    switch (dev_num)
    {
        case 0:
            pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;

            pctl->PCR[18] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;
            pctl->PCR[19] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;

            sim->SCGC4 |= SIM_SCGC4_IIC2_MASK ;

            break;
        case 1: //I2C1, LP Added 7/25/13
            pctl = (PORT_MemMapPtr)PORTF_BASE_PTR;

            pctl->PCR[3] = PORT_PCR_MUX(2) | PORT_PCR_ODE_MASK | PORT_PCR_ISF_MASK; // PTF3, I2C1_SDA, LP Added 7/25/13
            pctl->PCR[2] = PORT_PCR_MUX(2) | PORT_PCR_ODE_MASK| PORT_PCR_ISF_MASK; // PTF2, I2C1_SCL, LP Added 7/25/13

            sim->SCGC4 |= SIM_SCGC4_IIC1_MASK ; //Clock Gate, LP Updated 7/31/13

            break;
        default:
            /* Do nothing if bad dev_num was selected */
            return -1;
    }
    return MQX_OK;

}

0 件の賞賛
返信
3,038件の閲覧回数
leepenn
Contributor III

I did notice my Muxing was wrong, I updated that as below, but still same interrupt happening.

_mqx_int _bsp_i2c_io_init
(
    uint_32 dev_num
)
{

    PORT_MemMapPtr  pctl;
    SIM_MemMapPtr sim = SIM_BASE_PTR;

    switch (dev_num)
    {
        case 0:
            pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;

            pctl->PCR[18] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;
            pctl->PCR[19] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;

            sim->SCGC4 |= SIM_SCGC4_IIC2_MASK ;

            break;
        case 1: //I2C1, LP Added 7/25/13
            pctl = (PORT_MemMapPtr)PORTF_BASE_PTR;

            pctl->PCR[3] = PORT_PCR_MUX(2) | PORT_PCR_ODE_MASK ; // PTF3, I2C1_SDA, LP Added 7/25/13
            pctl->PCR[2] = PORT_PCR_MUX(2) | PORT_PCR_ODE_MASK; // PTF2, I2C1_SCL, LP Added 7/25/13

            sim->SCGC4 |= SIM_SCGC4_IIC2_MASK ;

            break;
        default:
            /* Do nothing if bad dev_num was selected */
            return -1;
    }
    return MQX_OK;

}

0 件の賞賛
返信
3,038件の閲覧回数
c0170
Senior Contributor III

Hello Lee Penn,

what interrupt is invoked??  Where do you enable clocks for PORTE and PORTF? Please provide some additional details, anything which might help us.

Regards,

0xc0170

0 件の賞賛
返信
3,038件の閲覧回数
leepenn
Contributor III

As part of the BSP, the clocks are all done in the _bsp_gpio_io_init for all ports. I am not sure how to determine which interrupt is being invoked, just that I end up in the _int_kernel_isr function when trying to initialize the I2C1 port. I am using exact same functions for I2C0 as I2C1.

0 件の賞賛
返信