Hi,
Please check the below example code, this may helps!
#include
#include
#include
#include "test.h"
#ifndef PSP_MQX_CPU_IS_KINETIS
#include
#endif
#if ! BSPCFG_ENABLE_IO_SUBSYSTEM
#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.
#endif
#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED
#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.
#endif
LWEVENT_STRUCT event;
/* Task template list */
TASK_TEMPLATE_STRUCT MQX_template_list[] = {
{ MAIN_TASK, Main_Task, 1000L, 9L, "Main task", MQX_AUTO_START_TASK},
{ TX_TASK, Tx_Task, 1000L, 8L, "TX task", 0, 0, 0},
{ RX_TASK, Rx_Task, 1000L, 8L, "RX task", 0, 0, 0},
{ 0L, 0L, 0L, 0L, 0L, 0L }
};
#if PSP_MQX_CPU_IS_KINETIS
void MY_FLEXCAN_ISR
(
/* [IN] FlexCAN base address */
pointer can_ptr
)
{
volatile CAN_MemMapPtr can_reg_ptr;
vuint_32 tmp_reg;
vuint_32 temp;
can_reg_ptr = (CAN_MemMapPtr)can_ptr;
/* get the interrupt flag */
tmp_reg = (can_reg_ptr->IFLAG1 & CAN_IMASK1_BUFLM_MASK);
// check Tx/Rx interrupt flag and clear the interrupt
if(tmp_reg){
/* clear the interrupt and unlock message buffer */
/* Start CR# 1751 */
_lwevent_set(&event, tmp_reg);
can_reg_ptr->IFLAG1 |= tmp_reg;
/* End CR# 1751 */
temp = can_reg_ptr->TIMER;
}/* Endif */
// Clear all other interrupts in ERRSTAT register (Error, Busoff, Wakeup)
tmp_reg = can_reg_ptr->ESR1;
if(tmp_reg & FLEXCAN_ALL_INT){
/* Start CR# 1751 */
can_reg_ptr->ESR1 |= (tmp_reg & FLEXCAN_ALL_INT);
/* End CR# 1751 */
} /* Endif */
return;
}
#else
void MY_FLEXCAN_ISR
(
/* [IN] FlexCAN base address */
pointer can_ptr
)
{
volatile FLEXCAN_REG_STRUCT_PTR can_reg_ptr;
vuint_32 tmp_reg;
vuint_32 temp;
can_reg_ptr = (FLEXCAN_REG_STRUCT_PTR)can_ptr;
/* get the interrupt flag */
tmp_reg = (can_reg_ptr->IFLAG & FLEXCAN_IMASK_VALUE);
// check Tx/Rx interrupt flag and clear the interrupt
if(tmp_reg){
/* clear the interrupt and unlock message buffer */
/* Start CR# 1751 */
_lwevent_set(&event, tmp_reg);
can_reg_ptr->IFLAG |= tmp_reg;
/* End CR# 1751 */
temp = can_reg_ptr->TIMER;
}/* Endif */
// Clear all other interrupts in ERRSTAT register (Error, Busoff, Wakeup)
tmp_reg = can_reg_ptr->ERRSTAT;
if(tmp_reg & FLEXCAN_ALL_INT){
/* Start CR# 1751 */
can_reg_ptr->ERRSTAT |= (tmp_reg & FLEXCAN_ALL_INT);
/* End CR# 1751 */
} /* Endif */
return;
}
#endif
/*TASK*-----------------------------------------------------------
*
* Task Name : Main_Task
* Comments :
*
*
*END*-----------------------------------------------------------*/
void Main_Task(uint_32 parameter)
{ /* Body */
_task_id created_task;
uint_32 result;
_int_install_unexpected_isr();
if (_bsp_flexcan_io_init(CAN_DEVICE) != 0)
{
printf ("\nError initializing pins for FlexCAN device %d!\n", CAN_DEVICE);
_task_block();
}
printf("\n*********FLEXCAN TEST PROGRAM.*********");
printf("\n Message format: Standard (11 bit id)");
printf("\n Message buffer 0 used for Tx and Rx.");
printf("\n Interrupt Mode: Enabled");
printf("\n Operation Mode: TX and RX --> Normal");
printf("\n***************************************\n");
printf("\nselected frequency (Kbps) is: %d", frequency);
data_len_code = 1;
printf("\nData length: %d", data_len_code);
| /* Select message format */ | format = FLEXCAN_STANDARD; | | /* Select mailbox number */ | RX_mailbox_num = 0; | TX_mailbox_num = 1; | RX_remote_mailbox_num = 2; |
TX_remote_mailbox_num = 3;
RX_identifier = 0x123;
TX_identifier = 0x123;
RX_remote_identifier = 0x0F0;
TX_remote_identifier = 0x0F0;
/* We use default settings */
bit_timing0 = bit_timing1 = 0;
/* Select operation mode */
flexcan_mode = FLEXCAN_LOOPBK_MODE;
/* Enable interrupt */
interrupt = FLEXCAN_ENABLE;
/* Enable error interrupt */
flexcan_error_interrupt = 1;
/* Reset FLEXCAN device */
result = FLEXCAN_Softreset ( CAN_DEVICE);
printf("\nFLEXCAN reset. result: 0x%lx", result);
/* Initialize FLEXCAN device */
result = FLEXCAN_Initialize ( CAN_DEVICE, bit_timing0, bit_timing1, frequency, FLEXCAN_IPBUS_CLK);
printf("\nFLEXCAN initilization. result: 0x%lx", result);
/* Select mode */
result = FLEXCAN_Select_mode( CAN_DEVICE, flexcan_mode);
printf("\nFLEXCAN mode selected. result: 0x%lx", result);
result = FLEXCAN_Set_global_stdmask (CAN_DEVICE, 0xFFF );
printf("\nFLEXCAN global mask. result: 0x%lx", result);
/* Enable error interrupts */
if(flexcan_error_interrupt == 1)
{
result = FLEXCAN_Install_isr_err_int( CAN_DEVICE, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN Error ISR install, result: 0x%lx", result);
result = FLEXCAN_Install_isr_boff_int( CAN_DEVICE, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN Bus off ISR install, result: 0x%lx", result);
result = FLEXCAN_Error_int_enable(CAN_DEVICE);
printf("\nFLEXCAN error interrupt enable. result: 0x%lx", result);
}
/* Set up an event group */
result = _lwevent_create(&event, LWEVENT_AUTO_CLEAR);
if (result != MQX_OK) {
printf("\nCannot create lwevent");
}
created_task = _task_create(0, RX_TASK, 0);
if (created_task == MQX_NULL_TASK_ID)
{
printf("\nRx task: task creation failed.");
}
created_task = _task_create(0, TX_TASK, 0);
if (created_task == MQX_NULL_TASK_ID)
{
printf("\nTx task: task creation failed.");
}
/* Start FLEXCAN */
result = FLEXCAN_Start(CAN_DEVICE);
printf("\nFLEXCAN started. result: 0x%lx", result);
// start the ping pong
while(1){}
} /* EndBody */
/*TASK*-----------------------------------------------------------
*
* Task Name : Tx_Task
* Comments :
*
*
*END*-----------------------------------------------------------*/
void Tx_Task(uint_32 parameter)
{/* Body */
uchar data = 0;
uint_32 result;
uchar string[] =
{
0xa, 0xb, 0xe, 0xc, 0xe, 0xd, 0xa, 0x0
};
result = FLEXCAN_Initialize_mailbox( CAN_DEVICE, TX_remote_mailbox_num, TX_remote_identifier,
8, FLEXCAN_TX, format,
interrupt);
printf("\nFLEXCAN tx remote mailbox initialization. result: 0x%lx", result);
/* Initialize mailbox */
result = FLEXCAN_Initialize_mailbox( CAN_DEVICE, TX_mailbox_num, TX_identifier,
data_len_code, FLEXCAN_TX, format,
interrupt);
printf("\nFLEXCAN tx mailbox initialization. result: 0x%lx", result); printf("\nFLEXCAN tx mailbox activation. result: 0x%lx", result);
/* Install ISR */
if(interrupt == FLEXCAN_ENABLE)
{
result = FLEXCAN_Install_isr( CAN_DEVICE, TX_mailbox_num, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN TX ISR install. result: 0x%lx", result);
result = FLEXCAN_Install_isr( CAN_DEVICE, TX_remote_mailbox_num, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN TX remote ISR install. result: 0x%lx", result);
}
/* Let Rx Task start to initialize */
_time_delay(1000);
result = FLEXCAN_Tx_message(CAN_DEVICE, TX_mailbox_num, TX_identifier,
format, data_len_code, &data);
if(result != FLEXCAN_OK)
printf("\nTransmit error. Error Code: 0x%lx", result);
else
printf("\nData transmit: %d", data);
while(1)
{
/* Let Rx Task receive message */
_time_delay(1000);
data++;
result = FLEXCAN_Tx_mailbox(CAN_DEVICE, TX_mailbox_num, &data);
if(result != FLEXCAN_OK)
printf("\nTransmit error. Error Code: 0x%lx", result);
else
printf("\nData transmit: %d", data);
string[7] = data;
result = FLEXCAN_Update_message(CAN_DEVICE, string, 8, format, TX_remote_mailbox_num);
printf("\nFLEXCAN tx update message. result: 0x%lx", result);
}
} /* EndBody */
/*TASK*-----------------------------------------------------------
*
* Task Name : Rx_Task
* Comments :
*
*
*END*-----------------------------------------------------------*/
void Rx_Task(uint_32 parameter)
{/* Body */
uchar dptr[8];
uint_32 result;
uint_32 DLC = 0;
uint_32 ID = 0;
result = FLEXCAN_Initialize_mailbox( CAN_DEVICE, RX_remote_mailbox_num, RX_remote_identifier,
8, FLEXCAN_TX, format,
interrupt);
printf("\nFLEXCAN rx remote mailbox initialization. result: 0x%lx", result);
/* Initialize mailbox */
result = FLEXCAN_Initialize_mailbox( CAN_DEVICE, RX_mailbox_num, RX_identifier,
data_len_code, FLEXCAN_RX, format,
interrupt);
printf("\nFLEXCAN rx mailbox initialization. result: 0x%lx", result);
result = FLEXCAN_Activate_mailbox(CAN_DEVICE, RX_mailbox_num, FLEXCAN_RX_MSG_BUFFER_EMPTY);
printf("\nFLEXCAN mailbox activation. result: 0x%lx", result);
/* Install ISR */
if(interrupt == FLEXCAN_ENABLE)
{
result = FLEXCAN_Install_isr( CAN_DEVICE, RX_mailbox_num, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN RX ISR install. result: 0x%lx", result);
result = FLEXCAN_Install_isr( CAN_DEVICE, RX_remote_mailbox_num, (pointer)MY_FLEXCAN_ISR );
printf("\nFLEXCAN RX remote ISR install. result: 0x%lx", result);
}
if (_lwevent_wait_ticks(&event, 1 << RX_mailbox_num, FALSE, 0) != MQX_OK) {
printf("\nEvent Wait failed");
}
result = FLEXCAN_Lock_mailbox (CAN_DEVICE, RX_mailbox_num);
if(result != FLEXCAN_OK)
{
printf("\nLock mailbox failed. Error Code: 0x%lx", result);
}
result = FLEXCAN_Rx_message(CAN_DEVICE, RX_mailbox_num, &ID, format,
&DLC, &dptr, interrupt);
if(result != FLEXCAN_OK)
printf("\nReceived error. Error Code: 0x%lx", result);
else
{
printf("\nReceived data: ");
for (result = 0; result < DLC; result++) printf ("0x%x ", dptr[result]);
printf("\nID is: 0x%x", ID);
printf("\nDLC is: 0x%x\n", DLC);
}
result = FLEXCAN_Unlock_mailbox (CAN_DEVICE);
if(result != FLEXCAN_OK)
{
printf("\nUnlock mailbox failed. Error Code: 0x%lx", result);
}
while(1)
{
if (_lwevent_wait_ticks(&event, 1 << RX_mailbox_num, FALSE, 0) != MQX_OK) {
printf("\nEvent Wait failed");
}
result = FLEXCAN_Lock_mailbox (CAN_DEVICE, RX_mailbox_num);
if(result != FLEXCAN_OK)
{
printf("\nLock mailbox failed. Error Code: 0x%lx", result);
}
result = FLEXCAN_Rx_message(CAN_DEVICE, RX_mailbox_num, &ID, format,
&DLC, &dptr, interrupt);
if(result != FLEXCAN_OK)
printf("\nReceived error. Error Code: 0x%lx", result);
else
{
printf("\nReceived data: ");
for (result = 0; result < DLC; result++) printf ("0x%x ", dptr[result]);
printf("\nID is: 0x%x", ID);
printf("\nDLC is: 0x%x\n", DLC);
}
result = FLEXCAN_Unlock_mailbox (CAN_DEVICE);
if(result != FLEXCAN_OK)
{
printf("\nUnlock mailbox failed. Error Code: 0x%lx", result);
}
FLEXCAN_Request_message (CAN_DEVICE, RX_remote_mailbox_num, format);
}
} /* EndBody */
/* EOF */
| result = FLEXCAN_Activate_mailbox(CAN_DEVICE, TX_mailbox_num, FLEXCAN_TX_MSG_BUFFER_NOT_ACTIVE); |
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------