How use fprintf or fputs to send a zero hexadecimal.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How use fprintf or fputs to send a zero hexadecimal.

Jump to solution
1,736 Views
jesusayala
Contributor I

i'm trying to send to serial port the next 

char data[] = {0x02, 0xa3, 0x08, 0x00, 0xab}; 

fprintf(serial_fd,  string); 

But only the three first bytes was send. If change the 0x00 for other value all data is sent. 

I think that the fprintf takes the 0x00 as a end of line.  How i can send the 0x00 value using fprint or fputs function?

0 Kudos
Reply
1 Solution
1,505 Views
issekiamp
Contributor I

How about using write() function instead?

See section 2.3 and 2.9.4 of I/O Drivers User's Manual for more information.

View solution in original post

0 Kudos
Reply
3 Replies
1,505 Views
soledad
NXP Employee
NXP Employee

Hello Jesus,

In fact if you are using "string" to send the information in the fprintf, you are going to loose the data of your array since the end of string is the NULL character which it is 0x00.

You need to send the byte to byte in a single loop to send all the data from the array


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,506 Views
issekiamp
Contributor I

How about using write() function instead?

See section 2.3 and 2.9.4 of I/O Drivers User's Manual for more information.

0 Kudos
Reply
1,505 Views
jesusayala
Contributor I

It works!

Thanks for your help.

:smileyhappy:

0 Kudos
Reply