How to set up BSP for PEx in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set up BSP for PEx in KDS

1,316件の閲覧回数
Vagni
Contributor IV

In MQX 4.1.1 the pe_demo project is provided also for KDS build configuration, but no PEx project is present in the KDS build configuration for the BSP library (the PEx project for BSP is present only in CW build configuration).

The MQX_BSP_Porting_Example_User_Guide document describes how to set up BSP for PEx with IAR or KEIL build environment.

What about KDS? How can I set up BSP for PEx in KDS build environment? Is there a setup procedure as for IAR and KEIL?

The pe_demo application needs a PEx-based BSP to run...

タグ(4)
0 件の賞賛
返信
2 返答(返信)

967件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Alessandro,

Marek is correct that the KDS/KSDK environment for MQX is quite different than the MQX classic implementation.

Please review some of these trainings:

MQX RTOS Training

You can create a new Kinetis Design Studio project for KSDK and include PE (Processor Expert).  PE has MQX Component that can be configured for MQX or MQXLite.

Regards,

David

0 件の賞賛
返信

967件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I am sorry the KDS is not still supported in the MQX (BSP projects are not provided for KDS yet).

I am moving this issue to MQX community because it is a question for the MQX support team.

Best Regards,

Marek Neuzil

0 件の賞賛
返信