How to open the webpage?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to open the webpage?

跳至解决方案
2,765 次查看
winmaxi
Contributor I

Hi, I'm currently reading the code of LAB 4.

 

How does the code link to the webpage it opens?

 

In the code there is <server = httpd_server_init((HTTPD_ROOT_DIR_STRUCT*)root_dir, "\\mqx.html");>   I can't locate mqx.html.

 

Also, could you please tell me how does it go to the root directory of the webpage without spelling out the webpage's address?

 

Thank you.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,795 次查看
M_ttferrari
Contributor III

HI, 

 

Are you installed the tfs? 

 

You need convert your web pages to tfs with mktfs.exe (it is located in somewhere at mqx folder, I don't remember now). This application converts your web pages into a c file (tfs_data.c) then you need to declare a HTTP_ROOT_DIR_STRUCT 

 

const HTTP_ROOT_DIR_STRUCT root_dir[] = {

 { "", "tfs:"},

 { 0, 0}

};

 

then before to install your server, install the tfs where the server will find your web pages (and images if you web page has ones).

 

io_tfs_anstall("tfs", tfs_data);

 

Please, take a sight to MQX RTCS user guide you will find some examples about how initialize a web server.

 

Matt

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,795 次查看
winmaxi
Contributor I

Now I know where the mqx.html locate. But I still don't know how the program indicate where the folder is without spelling out the directory.

 

Could anyone answer my question?

 

Thank you

0 项奖励
回复
1,796 次查看
M_ttferrari
Contributor III

HI, 

 

Are you installed the tfs? 

 

You need convert your web pages to tfs with mktfs.exe (it is located in somewhere at mqx folder, I don't remember now). This application converts your web pages into a c file (tfs_data.c) then you need to declare a HTTP_ROOT_DIR_STRUCT 

 

const HTTP_ROOT_DIR_STRUCT root_dir[] = {

 { "", "tfs:"},

 { 0, 0}

};

 

then before to install your server, install the tfs where the server will find your web pages (and images if you web page has ones).

 

io_tfs_anstall("tfs", tfs_data);

 

Please, take a sight to MQX RTCS user guide you will find some examples about how initialize a web server.

 

Matt

0 项奖励
回复
1,795 次查看
winmaxi
Contributor I

Thank you very much.

 

I have question about using mktfs.exe.

When I double click it directly, it will close in about 2 seconds.

When I run it using windows command prompt, what the format is like?

In using MQXlibraries document, 

it asks us to input like the following:

 

mktfs.exe <Folder to be converted> <Output source file name>

for example:

C:\mktfs.exe web_pages tfs_data_file.c

 

I put mktfs.exe C:.../webpages(the directory of the webpage folder) tfs_data_file.c

it asks me to input [-s <separate file>] <input_directory>

I don't know what it means, so I input as the folliowing:

 

mktfs.exe C:.../webpages(the directory of the webpage folder) C:..../tfs_data_file.c(where I want to save the translated C document)

it shows the same message.

 

What exactly the format should be like? Could anyone help me?

0 项奖励
回复