How to import a Project via .wsd file through command line.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to import a Project via .wsd file through command line.

2,052 Views
rossrhone
Contributor III

Is there a way to import a Project file via command line argument in Codewarrior 10.4 microprocessors? Example I want to import a project.wsd file and then be able to build the entire workspace via command line.

Thanks,

Ross

0 Kudos
Reply
3 Replies

1,705 Views
soledad
NXP Employee
NXP Employee

Hello Ross,

Please check the attached document. In addition please check the below video.

Video Link : 3373


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,705 Views
rossrhone
Contributor III

I believe I asked this question in the wrong area. I have codewarrior 10.4 for micro controller not MQX.

0 Kudos
Reply

1,705 Views
soledad
NXP Employee
NXP Employee

Hi,

Then please check the below link:

https://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

I hope this helps !!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply