How to get task ID from MQX watchdog failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get task ID from MQX watchdog failure

Jump to solution
2,264 Views
rvigneault
Contributor III

Hi,

We are using the watchdog of MQX 4.2 to detect crashes or halted tasks but I would like to know what information is available when the watchdog error function is called.

We are creating the watchdog using

if(_watchdog_create_component(BSP_TIMER_INTERRUPT_VECTOR, handle_watchdog_expiry) != MQX_OK)
{
   printf("\nError creating watchdog component.");
   _task_block();
}

where handle_watchdog_expiry is defined as

void handle_watchdog_expiry(void* td_ptr)
{
   printf("Expired task 0x%P\n\r", td_ptr);

    // Trig the hardware WDT
    while(1);
}

The declaration follows the function pointer type definition

typedef void (_CODE_PTR_  WATCHDOG_ERROR_FPTR)(void *);

used in

extern _mqx_uint _watchdog_create_component(_mqx_uint, WATCHDOG_ERROR_FPTR);

When I print the parameter given as a void pointer, I cannot find anything into the code to match the task to.

Is it possible to cast the void pointer into some struct from which useful information could be obtained?

If not, how can I use the pointer to match to a task?

Thanks

Tags (2)
0 Kudos
Reply
1 Solution
1,958 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Rudy

MQX watchdog component provides a software watchdog for each task. If a single task starves or runs beyond certain timing constraints, the watchdong provides a way to detect the problem. Initially, the task starts its watchdog with a specific time value, and if the task fails to stop or restart the watchdog  before that time expires, MQX calls a processor-unique, application-supplied expiry function that can initiate error recovery.

From the td_ptr, it is a pointer to the task descriptor of the task, it contains various information about the state of the task.

typedef struct   td_struct
{
   /*!
    * \brief A pointer to the next TD in the queue (for whatever queue this
    * task is currently in).
    *
    * This field MUST be the first field in the TD.
    */
   struct td_struct                 *TD_NEXT;

   /*!
    * \brief A pointer to the previous TD in the queue (for whatever queue this
    * task is currently in).
    */
   struct td_struct                 *TD_PREV;

   /*! \brief The current state that this task is in. */
   _mqx_uint                         STATE;

   /*! \brief The Task id of the task that this task descriptor represents. */
   _task_id                          TASK_ID;

   /*! \brief The Start of the Stack. */
   void                             *STACK_BASE;

   /*!
    * \brief If the task is blocked, then this is a pointer to the task's current
    * stack value, otherwise it is a pointer to the task's stack at the time of
    * the last block.
    */
   void                             *STACK_PTR;

   /*! \brief The other end of the Stack. */
   void                             *STACK_LIMIT;

   /*! \brief The Ready Queue upon which to place the task, when it is ready to run. */
   struct ready_q_struct            *MY_QUEUE;

...

...

}

you can get task id by this function

_task_id     _task_get_id_from_td(void * td_ptr);

Regards

Daniel

View solution in original post

3 Replies
1,959 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Rudy

MQX watchdog component provides a software watchdog for each task. If a single task starves or runs beyond certain timing constraints, the watchdong provides a way to detect the problem. Initially, the task starts its watchdog with a specific time value, and if the task fails to stop or restart the watchdog  before that time expires, MQX calls a processor-unique, application-supplied expiry function that can initiate error recovery.

From the td_ptr, it is a pointer to the task descriptor of the task, it contains various information about the state of the task.

typedef struct   td_struct
{
   /*!
    * \brief A pointer to the next TD in the queue (for whatever queue this
    * task is currently in).
    *
    * This field MUST be the first field in the TD.
    */
   struct td_struct                 *TD_NEXT;

   /*!
    * \brief A pointer to the previous TD in the queue (for whatever queue this
    * task is currently in).
    */
   struct td_struct                 *TD_PREV;

   /*! \brief The current state that this task is in. */
   _mqx_uint                         STATE;

   /*! \brief The Task id of the task that this task descriptor represents. */
   _task_id                          TASK_ID;

   /*! \brief The Start of the Stack. */
   void                             *STACK_BASE;

   /*!
    * \brief If the task is blocked, then this is a pointer to the task's current
    * stack value, otherwise it is a pointer to the task's stack at the time of
    * the last block.
    */
   void                             *STACK_PTR;

   /*! \brief The other end of the Stack. */
   void                             *STACK_LIMIT;

   /*! \brief The Ready Queue upon which to place the task, when it is ready to run. */
   struct ready_q_struct            *MY_QUEUE;

...

...

}

you can get task id by this function

_task_id     _task_get_id_from_td(void * td_ptr);

Regards

Daniel

1,958 Views
rvigneault
Contributor III

Hi danielchen@fsl‌,

This is exactly what I was looking for.

Thanks a lot!!

Rudy

0 Kudos
Reply
1,958 Views
danielchen
NXP TechSupport
NXP TechSupport

You are welcome and thank you for your update.

Regards

Daniel

0 Kudos
Reply