How to download MQX source for Linux Host?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download MQX source for Linux Host?

ソリューションへジャンプ
2,225件の閲覧回数
blake_genes
Contributor II

I downloaded FSLMQXOS_3_6_2.exe, which is the MQX source.  However, I am developing on Linux and doubt that an EXE is the correct way to start.  How do I get sources for MQX that work with CW 10.1 running on Linux?

 

I tried installing the MQX .exe file on a windows machine, and copied it over to the linux machine.  But I can't get it to compile using CW 10.1.

 

So my question is how to get started with MQX running CW10.1 on Linux.  Hopefully there is a guide out there somewhere for this.

 

Thanks.

0 件の賞賛
返信
1 解決策
1,538件の閲覧回数
JerryR
Contributor II
0 件の賞賛
返信
3 返答(返信)
1,539件の閲覧回数
JerryR
Contributor II
0 件の賞賛
返信
1,538件の閲覧回数
JerryR
Contributor II
Soon I will prepare a paper on his experiences working under Linux. to work with the MQX suitable CW10.0. plug-in MQXWIZARD CW10.1 causes an error when creating a project MQX. To work is only suitable MQX kernel compiled in CW10. To get started you can use "lib" directory compiled into CW10 (Win).
0 件の賞賛
返信
1,538件の閲覧回数
RuiFaria
Contributor III

I had a very similar problem and the answer from support center was:

 

"CW10.1 does not support MQX 3.6. Please wait until our MQX 3.7 release which is in March 31. This version will be supported in CW10.1."

0 件の賞賛
返信