How to download MQX source for Linux Host?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to download MQX source for Linux Host?

跳至解决方案
2,230 次查看
blake_genes
Contributor II

I downloaded FSLMQXOS_3_6_2.exe, which is the MQX source.  However, I am developing on Linux and doubt that an EXE is the correct way to start.  How do I get sources for MQX that work with CW 10.1 running on Linux?

 

I tried installing the MQX .exe file on a windows machine, and copied it over to the linux machine.  But I can't get it to compile using CW 10.1.

 

So my question is how to get started with MQX running CW10.1 on Linux.  Hopefully there is a guide out there somewhere for this.

 

Thanks.

0 项奖励
回复
1 解答
1,543 次查看
JerryR
Contributor II
0 项奖励
回复
3 回复数
1,544 次查看
JerryR
Contributor II
0 项奖励
回复
1,543 次查看
JerryR
Contributor II
Soon I will prepare a paper on his experiences working under Linux. to work with the MQX suitable CW10.0. plug-in MQXWIZARD CW10.1 causes an error when creating a project MQX. To work is only suitable MQX kernel compiled in CW10. To get started you can use "lib" directory compiled into CW10 (Win).
0 项奖励
回复
1,543 次查看
RuiFaria
Contributor III

I had a very similar problem and the answer from support center was:

 

"CW10.1 does not support MQX 3.6. Please wait until our MQX 3.7 release which is in March 31. This version will be supported in CW10.1."

0 项奖励
回复