How to add MQX 4.2 project to codewarrior 10.6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add MQX 4.2 project to codewarrior 10.6?

Jump to solution
1,897 Views
shark
Contributor I

Hi,

Currently I just install MQX 4.2. Before I use MQX 4.1. I already install MQX 4.2. But it doesn't appear in my codewarrior.  How I can a create new project for MQX 4.2 using my codewarrior 10.6?

0 Kudos
Reply
1 Solution
1,211 Views
DavidS
NXP Employee
NXP Employee

Hi Muhamad,

Please do Help->Install New Software...

For Work work: click pull down to the right and select following:

FSL MCU Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/MCU10_6_4/com.freescale.mcu.updatesite

Then check all the modules to update you have on your system.  For mine it was following:

ScreenHunter_146 May. 15 11.12.gif

If you peek inside the MCU v10.6 Updates for MQX you will see reference to MQX4.2 that will be updated:

ScreenHunter_145 May. 15 11.11.gif

Restart CW10.6.4 and do File->MQX 4.2 Project

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
1,212 Views
DavidS
NXP Employee
NXP Employee

Hi Muhamad,

Please do Help->Install New Software...

For Work work: click pull down to the right and select following:

FSL MCU Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/MCU10_6_4/com.freescale.mcu.updatesite

Then check all the modules to update you have on your system.  For mine it was following:

ScreenHunter_146 May. 15 11.12.gif

If you peek inside the MCU v10.6 Updates for MQX you will see reference to MQX4.2 that will be updated:

ScreenHunter_145 May. 15 11.11.gif

Restart CW10.6.4 and do File->MQX 4.2 Project

Regards,

David

0 Kudos
Reply