How reset time-slice counter back to zero?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How reset time-slice counter back to zero?

ソリューションへジャンプ
1,533件の閲覧回数
troll
Contributor II

Hi 

 

I'm using a few tasks as TIME_SLICE (time-slice = 100 millisec) and one main task which create this time-slice tasks and next it is blocked.

 

When I have finished main task, sheduler time-slice counter is not zero. As result first task has a little bit time less then 100 millisec.

 

How can I reset this time-slice counter before sheduller will start first time-slice counter?

 

Thanks in advance.

Good Luck.

0 件の賞賛
返信
1 解決策
1,013件の閲覧回数
JuroV
NXP Employee
NXP Employee

 

Hi troll :smileyvery-happy:

 

scheduler time-slice is only a default value for time-slice. Don't bother with that.

 

You want to have the tasks run the same amount of time. In that case you need to start new task on the new re-scheduling caused by timer.

 

This is a bit complex issue, needs small hack, but you can do this.

 

1) create task queue, store it as global variable: suspended_tasks = _taskq_create(MQX_TASK_QUEUE_FIFO);

2) create new tasks with higher priority (= more important tasks) than the starter task: _task_create(0, TASK_ID, 0);

3) create some variable to signal that tasks are ready to run on following interrupt (see small hack below):    reinit_tasks_on_interrupts = 1;

4) after (3), the starting task should run in infinite loop and not to call any function that can make rescheduling (e.g. _task_wait or _lwsem_wait ), just waiting for interrupt: wait(1);

 

5) every new started task will do as first step sleep onto taks queue: _taskq_suspend(suspended_tasks);

small hack:

6) open _bsp_timer_isr() int init_bsp.c and make that  the signal from (3) will resume all sleeping tasks:  if (reinit_tasks_on_interrupts) {  _taskq_resume(suspended_tasks); } before _time_notify_kernel();

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,014件の閲覧回数
JuroV
NXP Employee
NXP Employee

 

Hi troll :smileyvery-happy:

 

scheduler time-slice is only a default value for time-slice. Don't bother with that.

 

You want to have the tasks run the same amount of time. In that case you need to start new task on the new re-scheduling caused by timer.

 

This is a bit complex issue, needs small hack, but you can do this.

 

1) create task queue, store it as global variable: suspended_tasks = _taskq_create(MQX_TASK_QUEUE_FIFO);

2) create new tasks with higher priority (= more important tasks) than the starter task: _task_create(0, TASK_ID, 0);

3) create some variable to signal that tasks are ready to run on following interrupt (see small hack below):    reinit_tasks_on_interrupts = 1;

4) after (3), the starting task should run in infinite loop and not to call any function that can make rescheduling (e.g. _task_wait or _lwsem_wait ), just waiting for interrupt: wait(1);

 

5) every new started task will do as first step sleep onto taks queue: _taskq_suspend(suspended_tasks);

small hack:

6) open _bsp_timer_isr() int init_bsp.c and make that  the signal from (3) will resume all sleeping tasks:  if (reinit_tasks_on_interrupts) {  _taskq_resume(suspended_tasks); } before _time_notify_kernel();

0 件の賞賛
返信