How do I create an MQX project in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I create an MQX project in KDS

跳至解决方案
2,274 次查看
kecart
Contributor III

I have installed KDS_1.1.1 and MQX 4.1.1.  I have imported the twrk60f120m workspace and built the libraries.  When I try to create a new project to use the MQX libraries, there is no obvious wizard or option that allows me to do that.  Is that handled differently in KDS than it is in CodeWarrior 10.6 or is it not possible yet?

标记 (3)
1 解答
1,868 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year. 

At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available.  Also, MQX project files for all libraries and examples will be available for KDS. 


Alice

Best Regards

在原帖中查看解决方案

5 回复数
1,868 次查看
soledad
NXP Employee
NXP Employee

Hi Kelly,

Unfortunately there is not an option in KDS wizard to create MQX for KSDK project, I recommend to make a copy of an existing demo or example and edit this project. You can find them in the following paths.

C:\Freescale\MQX_KSDK_1.0.0\demos

C:\Freescale\MQX_KSDK_1.0.0\rtos\mqx\mqx\examples

Hope this helps.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,868 次查看
kecart
Contributor III

Will this be an option in the near future?

0 项奖励
回复
1,869 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Official support of KDS in MQX is planned in MQX 4.2 & MQX 5.0 coming later this year. 

At that time MQX plug-ins for KDS (e.g. Task Aware Debug & New Project Wizard) will be available.  Also, MQX project files for all libraries and examples will be available for KDS. 


Alice

Best Regards

1,868 次查看
kecart
Contributor III

Glad to hear it is expected this year.  Will the BSPCloningWizard also be available to support MQX with KDS?

0 项奖励
回复
1,868 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi

Yes .:smileyhappy:

Alice

Best Regards

0 项奖励
回复